FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-28-2020 05:36 AM
Hello,
I installed the OPC UA Server 01V04 app on the CORE. When I try to connect with the UA Test Client to opc.tcp://192.168.1.1:4840 it tries for a few seconds and says "No Endpoints Found." It is the same behavior as if I entered the wrong IP address. But when I try this on a Virtual ctrlX CORE (with port forwarding), I get the expected list of security options and I am able to proceed with connection. Only with the real demo it is not working. Any ideas what I can try?
Best regards,
Brian
Solved! Go to Solution.
10-28-2020 06:30 AM
Hello,
it seems that the OPC UA server is not running. In 1.04 it was sometimes necessary to reinstall an app again. Can you try out this.
Best regards,
smueller
10-30-2020 04:34 PM
I uninstalled the app, reinstalled it and cycled power. Then the OPC UA Server was responding.
Thanks,
Brian