04-27-2022 11:22 PM
I've established a connection to an OPC UA Server running on a ctrlX Core, but some of the display name values within the PLC node of the DataLayer are incorrect. These autopopulate with the correct names when I connect to a virtual core.
Solved! Go to Solution.
04-28-2022 05:07 PM
Could you send us a system report or at least tell us which system and OPCUA server version you are using?
This is already working well for quite a time:
04-28-2022 08:08 PM - edited 04-28-2022 08:10 PM
04-29-2022 09:27 AM
We found that there is a problem with the older versions of the system and the OPCUA server 1.12.4.
Please update to the official release version 1.12.6 of the system and also the OPCUA Server 1.12.5.