03-28-2023 11:30 AM
Solved! Go to Solution.
03-29-2023 04:48 PM
What are the details of your application? ModbusTCP is not specific to ctrlX. All slip rings are also different. There will be a degredating in the signal, due to the slip ring, which may impact the data throughput on that TCP segment. Higher quality slip rings will have less degredation and thus perform better for the network. It is a function of the slip ring design: quality of the materials used, size/bore diameter, etc.
04-04-2023 06:35 AM
Dear AutomateSHANE, yes it is about the ModBUS TCP speed only which max. 100 Mbit/s for 100m. We will add-on ethernet switch for more than the required speed.