cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Is it possible to disable SecurityPolicy for the OpcUA server?

Is it possible to disable SecurityPolicy for the OpcUA server?

jlee979
Member

I'm currently trying to get FactoryIO to work with the core via OPC_UA, and I get the following error:
"The chosen security policy is not supported by the client to connect to the server". 
In the OPC UA Server App Manual It states that it is possible to set the SecurityPolicy to None, and it can be configured in the datalayer. 

jlee979_0-1629752673064.png

However, a post made a while back states that the server will always use an auth/encryption. 

jlee979_1-1629752771037.png

So is it possible? And if so, what and how should the settings in the datalayer be changed? 

2 REPLIES 2

DevME
Member

Hi,

it is possible to configure the ctrlX OPC UA Server with none Secure Endpoints.

The settings can be done via Datalayer or OPC UA. For that you need a configuration like that:

DevME_0-1630051675929.png

Then you need to restart the opc ua server.

Best regards!

 

Could you specifiy the formatting for the datalayer? All the variations i've tried were rejected, and the only solution I was able to get working was a PUT request with the following payload

jlee979_0-1630351388253.png

PS: more info is avaliable in the CtrlxCore runtime manual 

jlee979_0-1630351778066.png

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist