FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
01-25-2021 04:13 PM
How to connect CANopen components to an automation system with ctrlX CORE?
Solved! Go to Solution.
01-26-2021 08:24 AM - edited 02-10-2021 03:57 PM
At the moment we do not provide a CanOpen master in the ctrlX CORE.
We made successfully tests with a USB to Can adapter (R902602780) and a Can master setup with ROS. This driver should be available from release RM21.03 (version 1.8.x) on.
But this is not handled in our realtime scheduling, so we do not give any commitment to real time capabilities of this interface.
01-27-2021 09:34 AM
We are currently using a RS485 to MQTT gateway from ADFweb in combination with teh ctrlX core. This way we are adding support for RS485 devces.
I see ADFweb also hs a CAN gteway so thismight be a solution for you too.: https://www.adfweb.com/home/default.asp
You can concert to many different protocols so there might be one which fits you.
01-27-2021 09:43 AM
Please beware that you will always get some communication delays when using protocol converters/gateways.
07-15-2022 03:46 PM
Was the CodeSys library used for this USB to CAN test?
07-27-2022 02:20 PM
Like mentioned above an ROS snap was used for my tests. So no PLC was included.