08-02-2022 11:01 AM
Hi All,
I have installed license for Ethernet/IP scaner for ctrlX core.
How ever, when I add the node Ethernet/IP in PLC then I cant download because it informed me there is no license! (See attached picture)
Do you know this problem? please share with me.
Thank you!
Solved! Go to Solution.
08-02-2022 04:30 PM
Which PLC app licenses do you have on your ctrlX CORE? As you are using 3 Tasks you will at least need PLC Basic and PLC Standard. See store page "ctrlX CORE - PLC App":
ctrlX CORE - PLC Basic License
R911397817 - SWL-XC*-PLC-PLC**********-BANN
ctrlX CORE - PLC Standard License (add-on)
R911411765 - SWL-XC*-PLC-PLC**********-NNNN
08-03-2022 04:58 AM
Sorry CodeShapherd,
I need to confirm one more. As I am using multi-task, so I need standard license (Add-on) then I only need to upgrade from Basic license to Standard license => Only 01 license OR I need to install both Basic license and standard license?
Thank you!
08-03-2022 06:43 AM
You need both license. The basic PLC and the standart PLC add on license.
08-03-2022 08:09 AM
Yeah.
So the advanced license is the same. Need basic + standard + advace to use full functionality of ctrlX PLC.
But, do you know when we need Advanced license? As I understand Advanced license is to use with multi-core to optimize the cycle time or task handling, right? Is there any additional function of this kind of license?
Thanks.
08-03-2022 10:04 AM
You are right. If you want to use the "full" PLC you need all three.
Advanced is at the moment and like you mentioned for multi core usage only.