FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
a week ago - last edited a week ago
The CODESYS documentation suggests there are no limits on the number of connections for the ENIP connections with the CODESYS add-ons. I suspect the reality is that there are limits based on the RPI, processor and application requirements.
Is there any benchmarking with the ctrlX core hardware to better understand the limits?
CODESYS Manual https://store.codesys.com/media/n98_media_assets/files/2303000006-F/4/CODESYS%20EtherNetIP%20Adapter...
Monday
As the number of slaves connected are influencing the runtime of then PLC softstack indeed unlimited is not quite correct and depending on the hardware used.
The only benchmark I know are made with the CODESYS Profinet Controller soft stack on a ctrlX CORE X3 and is pointing out that 10 slaves are running fine but more will cause increased PLC cyclce times and can cause troubles.