FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
05-19-2023 04:58 PM
With Ethercat app version 1.20.0 I see the E4070/E4071 error continuously on the drives. I am using IndraDrive CS. Attached is a complete backup (extension chagned to txt because par would not upload). What is the reason for this? Is there a way to suppress it?
Solved! Go to Solution.
05-22-2023 08:44 AM - edited 05-22-2023 02:47 PM
By activating the details view of the diagnostic trace in ctrlX DRIVE Engineering some more information are available:
SCSB: EtherCat: Wrong master mailbox counter (Falscher Master Mailbox Counter)
CNTR: Initializing seriel interface / set communication parameter cannot be adjusted. (Initialisierung Serielle Schnittstelle / Vorgegebene Kommunikationsparameter können nicht eingestellt werden.)
Could you send us your IO configuration of the EtherCat master and a system report of the ctrlX CORE (can be done via the question mark symbol on the right top in the web UI)?
Also from communication point of view a wireshark measurement at the drive showing the error would be interesting.
05-26-2023 10:49 PM
@CodeShepherd, a system report is attached.
06-06-2023 06:40 PM
@CodeShepherd, any thoughts on this?
06-13-2023 07:29 AM
@aFouraker sorry for late reply because of vacation time in Germany. I will try to get an answer beginning of next week.
06-20-2023 09:48 AM
We are still investigating this problem and add new information as soon as available.
06-23-2023 09:32 AM
To sum the information up:
Does this bring technical issues for your application or is it more a not nice to see? As the release cycle of the firmware is quite long for the old devices it could take some time to implement changes.
06-27-2023 03:29 PM
It is not a technical issue as far as I can tell but it is a nuisance. Is there a way to turn it off on the drive?
07-24-2023 08:15 AM
Unfortunately these warning cannot be suppressed.