cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Connect ctrlX OPC UA Client with Siemens S7 OPC UA Server

yannic
Established Member

Connect ctrlX OPC UA Client with Siemens S7 OPC UA Server

Hello together,

how can I connect my ctrlX Core to my Siemens S7. In the S7 I release some variables from sensors (OPC UA Server). With them I want to work in the ctrlX. I created a OPC UA client on the ctrlX, but I get no connection to the IP address of the S7. It would be nice if someone can give me a step by step instruction for the connection between both devices. It could be also another third-party device (e.g. Beckhoff).

6 REPLIES 6
DevME
Member

Re: Connect ctrlX OPC UA Client with Siemens S7 OPC UA Server

Hi,

the configuration of ctrlX OPC UA Client has changed in version 1.10. So first it is necessary to know your version of the app.

Best regards!

yannic
Established Member

Re: Connect ctrlX OPC UA Client with Siemens S7 OPC UA Server

Hello, I use 1.10.

yannic
Established Member

Re: Connect ctrlX OPC UA Client with Siemens S7 OPC UA Server

Hey,

Now the connection to the S7 works fine. But after a reboot of the core there is no automatic reconnection possible. Are there any settings to change for auto reconnect?

 

CodeShepherd
Community Moderator

Re: Connect ctrlX OPC UA Client with Siemens S7 OPC UA Server

We checked with our R&D and at the moment there is no setting to trigger an auto reconnect to a server. This has to be done "by hand" e.g. with the PLC function blocks or via the Data Layer in the application that uses the client.

CodeShepherd
Community Moderator

Re: Connect ctrlX OPC UA Client with Siemens S7 OPC UA Server

You could also use an init script that executes commands after reboot. See this topic for further information.

maurusbien
Established Member

Re: Connect ctrlX OPC UA Client with Siemens S7 OPC UA Server

Hello,

I just created a short NodeRED Flow example how a reconnect to an OPC UA Server from the OPC UA Client App can be performed (Flow as .json file attached). Please read the comments in the flow before using.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist