12-08-2023 10:08 AM
Hello,
I am wondering why a "MessageDataStructure Array[1]" as shown in the example will not be shown within the Core DataLayer? Is this kind of attribute not supported by the OPC-UA Client / DataLayer App?
UAExpert situation:
Core DataLayer situation:
Thanks for your information!
Solved! Go to Solution.
12-12-2023 10:13 AM
Hello,
which version of the OPC UA Client app do you use? I see non PLC datatypes, like "LocalizedText", "DateTime" inside the structure.
These datatypes are supported with RM23.11 (version 2.04) and higher.
09-05-2024 11:49 AM
Are there any news? Can this topic be closed?
09-23-2024 04:35 PM
Hello @CodeShepherd ,
today we have tested the feature with the latest app release 2.4 / 2.6. Now it seems to work fine!
So we are going to close this topic.
Thank you for the support.
BR Markus.