03-10-2022 03:51 PM
I created a new library to use in a PLC project. But the added header an documentation looks quite strange when using in the PLC. What do I have to do?
Solved! Go to Solution.
03-10-2022 04:05 PM - edited 03-10-2022 04:06 PM
There is an official documentation available at CodeSys homepage:https://help.codesys.com/webapp/reSTOverview;product=LibDevSummary;version=3.5.17.0
To use it an additional function package called "CODESYS Library Documentation Support 4.0.0.0.package" has to be installed. This is part of the ctrlX WORKS installation package but is not automatically installed:
This has to be done by hand via the package manager in the ctrlX PLC Engineering:
04-05-2023 10:21 PM
As of ctrlX PLC Engineering 1.18.1, the CODESYS Library Documentation Support package may be installed directly from the (new) Add-on installer. See below.