cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

WebVisu: Screen not responding the commands after a while

WebVisu: Screen not responding the commands after a while

ericvergara
Occasional Contributor

Hello,

We have carried out a project with a ctrlX Core X3 with Webvisu and PLC and two WR21 RC7, 

In normal conditions the project is working but from time to time (sometimes it is after 4 hours / 8 hours or even a day) we cannot execute commands anymore, we can change between screens and log in and so on but the standard buttons as the Auto / Manual mode are not working anymore and the only way of solving this is to switch off/on the screen or unplugging and plugging again the ethernet cable,

I have checked the tasks and at some point the Visu_task exceeds the configured 200 ms task time. I do not know if this could be the root cause,

Does someone experienced this before?

Thank you,

1 REPLY 1

CodeShepherd
Community Moderator
Community Moderator

Dublicate of "WebVisu: Screen not responding the commands after a while". Further discussion will be done there. Please do not post same question in several forums. 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist