FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
09-21-2024 10:50 AM
Hello,
I am using softmotion solution to control my axis for jogging & positioning. while doing so, i had to read the actual velocity feedback of the axis running, which was always in-correct values.
How can i make these feedback values in-line with actual velocity feedback?
09-26-2024 08:12 AM
you must look in the dirve structure.
All target and actual values of the axis are available here
09-27-2024 04:33 AM
Hello,
Below is picture taken during a trails. while my set value is 10 the actual feedback is only 0.6. is possible to fix this gap?
10-18-2024 09:11 AM
Hello
I think that is a inkonsitece of your scalling or the Units.
Remeber that the softmotion works with units/sec and units is the IPO
a month ago
Hello,
Can you guide me, . How can i set the proper scaling for the softmotion based applications.
a month ago
Hello you must go in the PLC menu of the drives.
the value of the scaling is dependent on the settings of the axis these are the standard settings for a linear indradrive axis