Library Error when adding the Ethernet/IP Scanner

Library Error when adding the Ethernet/IP Scanner

ericvergara
Occasional Contributor

Hello,

When I add the Codesys Ethernet/Ip Scanner I can't download the project to the PLC, it pops up the following errors:

ericvergara_0-1655116442550.png

 

It seems that it is a library error, I have tried with the 3.5.17.0 IoDrvEthernetIpAdapter library version but it returns even more errors and the PLC project is empty, I have only added the Ethernet/Ip Scanner,

Does anyone know what should I do?

Thanks for the help,

5 REPLIES 5

ericvergara
Occasional Contributor

Any news regarding this?

HmiGuide
Community Moderator
Community Moderator

Which ctrlX works version are you using. In 1.12.9 RM21.11.7 I can't find this library.

ericvergara
Occasional Contributor

Hello HmiGuide,

I am using the RM22.03 version, this library is automatically inserted when the Ethernet/IP Scanner is added,

PLC2030
Long-established Member

It seems your project uses an older version of the Ethernet/IP libraries. A check of the library versions with RM 22.03 (01V14) should have the following result:

PLC2030_0-1658130011533.png

Did you install the Ethernet/IP package 4.2.0.0. from the ctrlX Collaboration Room?
If you already have Ethernet/IP package 4.2.0.0, please check whether the library in your project is set to an older version.

 

ericvergara
Occasional Contributor

Hello PLC2030,

Right, I reinstalled the Ethernet/IP package and then it worked,

Thanks!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist