Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Is there an OSCAT Network library supported in ctrlX Core?

Is there an OSCAT Network library supported in ctrlX Core?

ericvergara
Occasional Contributor

Hello,

We need to use the Network Oscat library and the problem is that with our current library version it comes up an error as the image shows below:

ericvergara_0-1652885041737.png

We have tried with a 32 bit PLC Application and it worked, so we assume that it is because the ctrlX Core is based on a 64 bit architecture,

Is there an alternative to this library? Does someone know if there is another version?

Thanks in advance,

5 REPLIES 5

CodeShepherd
Community Moderator
Community Moderator

ctrlX CORE is based on 64 bit operating system, yes.

The actual version of OSCAT available seems to be 1.10 and you are using 1.3 did you try to use the latest version?

ericvergara
Occasional Contributor

Hello CodeSheperd,

Thanks for your fast answer,

We don't know where to download this latest library, we are using the 1.3.5.2 version,

Do you know where can we find it?

 

PLC2030
Long-established Member
In the Codesys Store (https://store.codesys.com/de/oscat-network.html) the description of the library says that it is currently available for 32 bit systems only.

HmiGuide
Community Moderator
Community Moderator

The homepage of oscat is: http://www.oscat.de here you can find all infos and current versions of OSCAT libraries.

I don't know which network functionality you are using. The network library shipped by ctrlX is CXA_SocketComm.

ericvergara
Occasional Contributor

We want to execute FTP commands but I think that with the library that you just mentioned we can already do that,

Thanks!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist