02-09-2023 12:28 PM
Hello,
When we add the "Write variable" as a command for an object and select any of the keyboards this keyboard comes with a predefined sizing,
Is it possible to make this keyboard even bigger?
Many thanks,
Solved! Go to Solution.
02-10-2023 09:10 AM
Here is an entry in CoDeSys forum:
https://forge.codesys.com/forge/talk/Engineering/thread/06797e219a/
02-17-2023 09:32 AM
02-10-2024 05:33 PM
Hi Eric,
When I try to use a solution similar to yours, it will open and allow me to enter some data into the keypad, but it crashes the open HMI page as soon as I hit "enter", "esc" etc. I assume it's failing to pass some data (maybe a string output?) back when the dialog closes.
Also, when I try to link the "Reference" to this Visulisation, it looks like the keypd is invalid. I have attached an image of this as a reference.
Does this sound familiar to you, and did you find any solution to it?
Thanks,
Nick
02-12-2024 08:59 AM
Hello Periapsis,
Hve you checked the actions of the "Esc", "Enter" and the rest of buttons?
Each button has his own action, for example the Enter does this:
I am sharing with you my own keypad so you can try it, if this works for you then you just need to select which one do you like more in Dialog Settings
Hope this helps,
Eric