05-18-2023 08:36 AM
Hello,
We have a customer that would like to use the EthernetIP adapter/scanner PLC addon on ctrlX Core, is there a project example available for this topic? Or detailed documentation on how to set it up?
Thanks
Solved! Go to Solution.
05-18-2023 04:28 PM
05-19-2023 07:52 AM
See also examples in our how to area.
05-19-2023 08:01 AM
I have watched the Ethernet/IP example, but it was not very helpful unfortunately as it does not show how to set the Adapter up, rather just a demo that the presenter got it working.
05-19-2023 08:13 AM
05-19-2023 08:24 AM
I went through the manual, but it does not show an example of how to set some data points for exchange, it is also outdated as v 1.20 does not have a Package Manager anymore, but Add-on installer instead, which has a bit different user interface.
Thank you so much for sending the presentation, it was well documented and I got it working as an EIP Scanner, please let me know if you come across something simimlar for the EIP Adapter.
05-22-2023 08:13 AM
05-22-2023 08:16 AM
You can refer to the CODESYS online help, too.