03-27-2023 03:25 PM
Hi,
The user of a ctrlX CORE setup with Ethernet/IP scanner has reported a situation of lost IP address.
The IO device connected via eth1 (using Ethernet/IP) reported no communications, Ethernet and EthernetIP scanner devices show "Not Running".
The user traced the issue to eth1 had lost the IP address settings configured during commissioning. No obvious diagnostics to highlight the issue other than "Not Running" message.
Is this a known issue?
For reference this is the same machine from the follow issue. Link
03-30-2023 03:48 PM
Hello,
which version of ctrlX CORE and Ethernet IP Add-On the customer is using?
kind regards
03-30-2023 04:55 PM
ctrlX CORE Versoin 1.12 (we plan on upgrading to 1.20 as soon as it's LTS).
Ethernet/IP package 4.2.0.0
03-31-2023 01:30 PM
Hi,
customer should test with the current CODESYS release 4.4.1.0.
kind regards
05-09-2023 08:54 AM
Hello,
any news from the customer?
kind regards