Dear all, I am trying to get a XCD1-W2323 working in single phase mode for desk testing. Unfortunately the drive doesn't want to apply power. In de mains connection monitoring the 230 volt connected to the mains input is showing correctly. But the drive doesn't charge the DC-bus. I tried configuring the supply unit in all the five possible options, see attached image. Up till this point we used an IndraDrive Cs as a DC-bus powersupply by connecting the DC-bus and connecting the BB contact on the XCD to an input on the IndraDrive. A small MLD program the evaluates the readiness and then sends a digital I/O signal to the ctrlX parameter S-0-0240 (see second attach image). This works well but is far from optimal. Could someone advice me how to get single phase operation working? For the sake off a 'clean' desk, easy testing and just wanting it to work.
... View more