Because of missing hardware that would be used as master to guaranty realtime (deterministic) communication it is not possible to use our EtherCat master app. Also keep in mind that the ctrlX COREvirtual must not be used in any productive environments/applications and automatically shuts down after 4h.
The only possibility would be to use softstacks like the CODESYS - Fieldbus Communication with restrictions in performance an deterministic. You will need at least ctrlX WORKS version 1.18 (see this thread).
... View more