I have installed on my PC, the CtrlX-Core (Virtual) V1.20.0. The target is to use this sevice to test and evaluate fieldbus (EtherCat and Profinet) connections to our tightening controllers. This means that the CtrlX-Core (Virtual) would require MASTER functions. Question: is the PC (laptop) based CtrlX-Core (Virtual) capable of supporting the above mentioned fieldbus MASTER functions? If YES, which APP's must be installed? Regards. UPDATE: Following correspondance with collegues, the EtherCat Master App may be installed BUT data cannot be exchanged with external devices (offline project generation only).
... View more