In the current version 2.02 of the ctrlX PLC Engineering you can find an import button to automatically create function blocks for acessing your self created fltbuffer.
ctrlX PLC Engineering - import from flatbuffer file
When a library needs to be created: In the 1.18 and 1.20 version of the SDK the PLC library creation mechanis and also the PLC export file are not working properly. Please use version 1.16 to create the library.
The parameter in the start.bat of 1.16 will inclued some "lib" (e.g. -libTitle) not fitting to the instruction that can be found here. But without changing the star.bat it schould be possible to import e.g. sampleSchema.fbs in an already opened library project.
In version 1.20 of ctrlX PLC Engineering there could be warning in the library project that CXA_Flatbuffers could not be resolved by using "*". As a workarround it can be set to 0.1.3.0 by hand.
... View more