Hi. I have a project configured on a CORE X3+ with in-line EtherCAT ctrlX IO (XF50) as well as Ethernet/IP to a camera device (XF51/eth1). I can talk to both of these individually. However, when the Ethernet/IP is active, the in-line ctrlX IO cards no longer respond. The cards are still in run state, but without any IO or indicators lighting. Dashboard and IO Engineering say EC is running without error. ETH/IP and EC are configured on different subnets. I can still talk to the camera through E/IP without problems. Any help would be greatly appreciated.
... View more