Hi, colleague and I are working on getting some sensor input into the ctrlX so we can process it with NodeRed. However, we're having trouble getting the sensors working, current roadblock is that we can't get the ethercat slave into OP mode. We're using a CtrlX CORE, linked to it is a WAGO 765 4202/0100 0000. We installed the .xml according to this and this guide; uploaded the configuration into our CORE, however we get this "error": The configuration we uploaded looks like this: In the slots we have plugged in: X01: Balluff X02: IMF with IO Link Adapter We tried installing the XML files for those two aswell, however when trying to install them in the repository an error would occur. Another thing we tried is to just get the WAGO Linkmaster running on its own with no attached devices, to no avail, same problem. We looked up different threads stating similiar problems, but couldn't find a solution that was applicable to our problem (at least we think so). We also looked into IO-Link compatibility, because the Master is Type B and the Sensors Type A, but our research claimed those should be compatible? (We're rookies) Thank you very much in advance for your help!
... View more