Hello, Thanks for your query... The DeviceBridge license count calculated based on Device or Tag count. 1 Device or 100 Tags = 1 License. If you have 2000 Tags in 1 device, then 20 license will calculated. If you have 5 device's and each device having 100 Tags, then the license counts is 5. If you have 2000 Tags ,if you distrubte into multiple device's (Ex: Device 1 - 1,000 , Device 2 - 500 , Device 3 - 100, Device 4 - 100, Device 5 - 100, Device 6 - 200), then the license counts is 20 ( Ex: Device 1 - 10 license, Device 2 - 5 license, Device 3 - 1 license, Device 4 - 1 license, Device 5 - 1 license, Device 6 - 2 license). If lincese available, yes you can add the more that 100 tags in 1 Device itself. Yes, you can use all the tags. Which is the maximum load (Devices & tags) each CtrlX can handle (X3, X5 & X7). Need more clarity on this questions? Yes, from DeviceBridge you can send the data to Nexeed MES system. You can find in connector -> Bosch -> Nexxed MES DDL and assign the IP address and Port number. Thanks Product Support
... View more