02-10-2022 11:18 AM - edited 02-10-2022 11:36 AM
Who connects complex processes, systems and applications and makes them quicker, simpler and easier to operate? From IoT solutions and Node-RED to the use of power functions for automating engineering routines.
In the category "Simplify engineering" four developers are competing against each other.
Two of them come from the United States, one is from Italy and one is from Austria.
And these are their ideas:
- Automation of measurement studies
Automation of the collection and evaluation of measurement studies using library functions.
- Digital twin via open source
Creation of the digital twin of a system based on open source software.
- System training through user instructions
Remote controlled car with camera that learns from the user's commands by using reactjs, nodejs, johnny-five and machine learning.
- Platform-independent IDE for PLCs
Integration of ctrlX PLC into a platform-independent PLC programming environment that can also be used to program systems from other manufacturers.
This thread can be used for all questions and discussions related to this category.