08-27-2020 01:53 PM
Hello colleagues,
how is it possible to start ctrlX DRIVE Engineering 1.06 (1.6.1) directly from Browser instead of version 1.04. (Link at EtherCAT / Status - See picture.
ctrlX Works 1.04 is installed: If I don't install the DRIVE Engineering component (from ctrl Works setup 1.04) and install the DRIVE Engineering 1.6.1 separately then the link in the browser doesn't find the DRIVE Engineering.
If I install the DRIVE Engineering as a component from WORKS 1.04 the according version DRIVE Engineering 1.04 starts from the a.m. link in the webpage EtherCAT/Status.
Regards, Stefan
Solved! Go to Solution.
09-03-2020 11:48 AM - edited 09-03-2020 03:24 PM
Hi Stefan,
in this way you can only start and open the ctrlX DRIVE Engineering Version you installed together and via your ctrlX WORKS installation.
A seperate installed version has to be started manually.
Best regards