Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

VHDX for virtual Core

VHDX for virtual Core

rum1
Established Member

Hello,

Is the VHDX format available for the virtual core and can it be used with it?

Kind regards!

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

The ctrlX COREvirtual is available as QEMU image only at the moment.

FooFighter
Long-established Member

Hello,

qemu supports to add vhdx files as additional storage (like an emulated usb-stick). Today this is not a part of the user interface support in ctrlX WORKS but can be created manually.
Here follows a brief description:

Create a virtual disk as usb-stick for ctlX COREvirtual

- Press Windows + X and select Disk Management.
- Click Action> Create VHD.
- Then go to "Browse".
- Specify the storage location and file name. (Example 'd:\usb-stick.vhd') (500 MB, format vhd, fixed size)
- The disk appears as a not initialized disk in the disk list, right click and choose initialze (GPT)
- Then select the unallocted space (484 MB) right click and select new simple volume click next next next and quick format with FAT32 (label USB-STICK)
- Now the disk is accessible with the assigned drive letter (add a test.txt file)
- Before starting the virtual control detach the vhd file in the diskmanagement dialog of your windows pc otherwise qemu can not access it

Attach the vhd file as usb stick to qemu

Open a virtual control batch file (e.g.: C:\ProgramData\Rexroth\ctrlX WORKS\virtual-controls\images\1.11.0-develop01323\tf0dtez3.user.qcow2.tap.start.bat)
Make a copy of the changed batch file and add the vhd file with the additional parameter '-drive file=d:\usb-stick.vhd,media=disk'
Start the virtual control (execute batch file)


Regards, Oliver

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist