FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
04-26-2021 11:41 AM
Hello
Last week the access to the controller worked perfectly
Now I geht this message
How should I switch the mode, if I can't get online
Pinging the Controller ist possilbe.
What can I do?
Thank you
Solved! Go to Solution.
04-26-2021 02:25 PM
Could you please tel us, what the last steps were before shutting down?
Did you try to empty your browser cache and connect to the control again?
What is light pipe flash code? Probably you are stuck while booting somewhere.
04-26-2021 02:53 PM
I switched off the power supply friday afternoon.
Before I updated the system apps to the actual versions and installed all apps coming from the download folder
On friday everything works perfect
I emptied the cache, but it did not help
The LED is flashing blue most of the time
Sometimes green and sometimes red.
Thank you for your help
04-29-2021 10:00 AM
Hi RainerFuchs,
in the current version we have an issue when the memory is full the DeviceAdmin App doesn't start anymore which ends up in the situation you describe.
This can happen when you have to many apps on your control, even older versions of one app count.
Or if you have an app which writes on the disk and fills it up.
For the Version 1.8.x or older you have the following possibilities.
If you have a root user and ssh enabled connect with ssh and delete apps.
If not you can together with you partner from Bosch Rexroth image the control or send it to the Service.
07-26-2021 02:01 PM
Hello,
I have exact the same problem here. I was upgrading my ctrlX from RM20.11 to RM21.03. I followed the ' RM 21.03 – Important update information ' carefully. Every step in he document was succesfully. But after step 9 I become a problem.
Step 9: 9. Update "Solutions XCR-V-0108.1.app" system app
After that, the ctrlX core was booting up automaticly. After that, the blue light stays flashing.
The ctrlX is pingable, and I see the core in the ctrlX Works. But double-clicking the core I get the message is in te attach. Waiting for hours has no result, also newstart has no effect. How can I solve this problem?
08-26-2021 04:02 PM
Any news on this or can the topic be closed?
09-07-2022 02:59 PM
Actually just 30 Minutes later it works again.