FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
12-01-2023 03:32 PM
I had a question regarding how to connect the virtual core to the internet because I have been trying to do this for a few days but it keeps giving me a timed out error in node red. I need the internet to install specific palettes such as the influx pallete that contains the influx nodes. I was following the instructions shown in the following link:
12-01-2023 04:31 PM - edited 12-04-2023 02:46 PM
Can you please let me know which of the following applies to your virtual core?
Depending on your set up, the required configuration will be different.
If you are able, connect your PC to a home network, disconnect from VPN, and place the virtual control in port forwarding mode (#1). You should have internet access at that point without the use of a proxy. This is the easiest method.
12-06-2023 10:11 AM
Hi,
Sorry for the late reply.
I was trying to make it work using method number 4 which is the 'Network adapter mode and PC is connected to home network (open internet)'.
I also tried doing the solution you gave which was to connect my PC to home network and port forward but it didn't work. The error it gave me is attached below which was; "RequestError: getaddrinfo EAI_AGAIN time.jsontest.com". Do I have to connect my PC to my router through ethernet to make it work or is a normal wifi connection enough.
Thanks for your time and help.
12-06-2023 02:32 PM
Wifi connection should be fine. Let's focus on method #1 for now.
Once you placed the control in port forwarding mode and on your home network, did you remove the proxy configuration on the control? I recieve a different error in Node-RED with the proxy enabled.
Are you using a VPN?
If you still recieve this error after disconnecting from VPN and disabling proxy in the control, could you please post an image of your virtual control network interface configuration?
12-06-2023 03:21 PM
Yes, I have removed my proxy configuration although it was in the disabled state and there is no vpn connection. I still get the EAI_AGAIN error in node -red. I have attached the images of the network interface configs.
12-06-2023 03:37 PM
Are you sure your Virtual Control is configured to Port Forwarding mode in ctrlX WORKS?
Can you please make sure this is the case and then try enabling DHCP for your ipv4 settings on the eth0 interface?
With a static IP of 192.168.1.1, it may be that your router is on a different subnet.
12-06-2023 04:07 PM
Probably we should arrange an online meeting to clarify things and check why the instructions in the how to did not help. Please send me a private message with your contact data so we can have a look together to your system.
12-06-2023 04:35 PM
It's solved!! I am able to connect to internet and was able to install the necessary palettes in node-red. The problem was that in my ctrlX WORKS like you said, port forwarding mode was not enabled, it was in the network adapter mode. This meant that even if i enabled port forwarding on my virtual control it would not connect. I did not know you had to or could even do that in the ctrlX WORKS as it is my first time working with CtrlX. Thanks a lot for the help. Life saver, was trying to get this working for a week. I attached image of the node-red working and where I had to go in the ctrlX WORKS to solve the issue.