FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
10-11-2024 03:33 AM
I am trying to communicate between Beijer and CORE X with Codesys ARTI.
I used the same symbol configuration as Indraworks,
but the communication is not working.
Do you have any experience interfacing to CtrlX core using Beijer?
10-18-2024 08:31 AM - edited 10-18-2024 08:33 AM
Like mentioned for other CODESYS V3 communication clients before, please beware that current versions are always using encrypted communication for security reasons. So the client connected to it also needs to be able to do so. See e.g. topic "communicate to 3rd party HMI via Codesys V3 protocol in ctrX PLC >=1.20" or also "Connect Weintek cMT2078X to ctrlX PLC via Codesys V3".