FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-06-2020 11:05 AM - last edited on 11-20-2020 09:46 AM by NorbiS
The motor can be selected by peak and/or continous torque values. This value can be insert as text or by slider control. The scale of the slider seems not to be convenient. Pls make available a more sensitive scale for lower torque range.
Proposal: linear scale from 0 to 10Nm, from 10 to 100Nm, and from 100Nm to end of scale.
Solved! Go to Solution.
10-07-2020 05:23 PM
Thank you for your suggestion👍. It is planned to optimize the usability of the sliders in a future release.