FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
09-06-2023 08:43 AM
Hi,
I´ve just wanted to configure my HW setup with COREX-M + IO modules.
As soon as I add IOs object to my project, there is always pre-configured Coupler module even I do not need it. It probably original comes from having only COREX-C HW but currently it´s not right.
Is there any way how to remove the coupler I could not find?
Thx. P.
Solved! Go to Solution.
09-06-2023 09:39 AM
If you have a ctrlX COREplus (e.g. COREX-M-X3) and make a connection to ctrlX IOs you can choose local bus connection.
09-06-2023 09:55 AM
Hi,
ok, that works. It´s not that intuitive that you have to create connection for it first.
I would prefer to have that decision directly in IO block, but probably just my opinion 🙂
Thanks a lot.
P.
06-04-2024 11:15 AM
Thank you for this post! Its helpful!
I would also suggest or like to have direct connection with IO modules when I have "Module extendable CtrlX Core" selected.
But he above solution worked for me thank you.
Thank you