cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Detail on Two-Handed control

Detail on Two-Handed control

bclapperton
New Contributor

Are there any further details on the SAFEX two handed control function block?

eg. Logic diagram, timing diagram, discrimination time between the two inputs, faults detected?

I am reluctant to use it with so little information provided. However, I also would prefer to use a pre-tested function block rather than write my own software. 

bclapperton_0-1716446035368.png

 

4 REPLIES 4

Dias
Community Moderator
Community Moderator

Hello Bruce,

there are no more details for Two-Hand Control. It is also not possible to deactivate the Cross Circuit you can do this but the wiring is always the same:

Dias_0-1718698544548.png

I made a test with this Configuration but nothing happen no function.

For the moment it is the best make your own User Group.

 

Dias
Community Moderator
Community Moderator

Hello Bruce,

I made some better test with the following result:

You can use just one Two Hand Control.
You can switch OFF the Cross Circuit Check it works but the wiring doesn`t change

This Inputs: 

Dias_0-1719480225133.png

leads to this Output

Dias_1-1719480252918.png

and this Inputs:

Dias_2-1719480360419.png

leads to this Output:

Dias_3-1719480392190.png

To the internal discrepence times I dont have actual information.

 

 

 

 

 

 

 

Dias
Community Moderator
Community Moderator

Hello Bruce,
now comes the information about the discrepance time I made some tests: The maximum discrepancetime is 500ms

Dias_0-1719489336052.png

 

Dias
Community Moderator
Community Moderator

The discrepance time is not configurable because the standard ISO 13851 sets the value at 0,5s

Dias_0-1722495001416.png

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist