09-24-2024 01:27 PM
Dear Community,
I had a problem with them PLC app when downloading an app and in another thread i was told that i have to upgrade or downgrade my apps and softwares. i have tried with the 2.6 versions and that didnt work maybe my core X3 doesnt have that and that i have to do a system image update. so what io did was that i decided to change everything to 1.20 versions.
all the apps worked but the PLC app i recieved this error:
The PLC app is currently not available (Error: 404)
This is most likely due to one of the following reasons:
the full error is in teh attachements.
thank you 🙂
09-24-2024 02:44 PM
Hello !
the licenses regarding ctrlX PLC Basic/Standard/Advanced/Performance in version 01VRS+ and 02VRS+ differ incompatible.
Means - the ctrlX PLC versions of 02VRS will run with a new license. please contact you license admin if not available.
Bye
09-24-2024 02:51 PM
See more information in the store area ctrlX AUTOMATION - PLC.
09-26-2024 12:54 PM
Hello,
i want the PLC 1.20 to be working, what do i need for that, in the first message you will find the screenshot for that