FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
02-17-2023 12:39 PM
Is there a way to synchronize multiple IL_TempControl FB's?
I am using up to ten FB's in a manual mode to generate PWM outputs. When the input to the different FB's is identital, I would like to get the ten synchronous PWM outputs. It seems the IL_TempControl doesn't have an input to synch.
All FB's run in the same task with a cycle time of 25 ms. The mean cycle in real is about 300 us and the max. < 700 us, if relevant...
Thanks!
Solved! Go to Solution.
04-14-2023 02:42 PM
Hi Venzi_,
this seems not to be possible at the moment.
But we will have a look at it, maybe it can be implemented in some future version.
Regards