FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
12-19-2023 02:18 PM
Hello.
I just updated my Core X3 to 1.20.6 as well as the PLC app
Sametime I also upgrade control X Works to new built 1.20.8
Afterwards I re-opened my PLC code and now recipe manager is missing!
Please advise on how to get it back
Thanks a lot
ps. Cant insert because I cant select a recipe manager
Thanks a lot
12-20-2023 07:12 AM
Did you already try to do a repair installation? Also uninstall and reinstall could help.
You can check out also "Error occurs when startup the IO Engineering". There some installation workarounds are mentioned.
12-20-2023 10:11 AM
Hello.
I tried repair as well es uninstall.
After uninstall it is impossible to re-install due to the following error:
Before uninstall I checked IO-Engineer which worked without any errors
12-20-2023 10:23 AM
Just checked. The mentioned file is missing inside the packege folder of the installation. Even fresh download still missing.
3 weeks ago
Is this still an issue or could it been solved on your side?