Problem with scaling and rotation of elements in visualization

Problem with scaling and rotation of elements in visualization

JoachimS
New Poster

I used some existing IndraLogic visualizations from IndraWorks 15. In IndraWorks it worked fine. If I reuse the stuff in ctrlX PLC engineering basically everything works except scaling and rotation of elements. I wonder why.
As far as I saw, we also use the old IndraLogic visualizations coming with the AxisInterface and I assume there are no problems. I appreciate your hints. 

6 REPLIES 6

Goldfinger
Established Member

Hello Joachim,

i have taken the AxisInterface visualzations from IWE into the new ctrlX world.

I do not remember any visualization specific problems.

Maybe you can describe your problems a bit more in detail....

Best regards,

Klaus

The problem is quite simple: As visualization element there is just a straight line. I want this line to rotate. For this reason I enter in the properties "Absolute movement/Rotation" a local variable or a global one. But there is no movement. I experienced the same with Scaling.  

Goldfinger
Established Member

There is only one point with a moving element in the AxisInterface visualizations:

Goldfinger_0-1613997167157.png

I did no changes here in IWE and ctrlX the last years.

You can look into the details. Just add the library CXA_MotionInterfaceUser to your project.

Right mouse-click on the library and select "Export library". As this is delivered as an open library, you can open it wiht PLC Engineering and have a closer look into the element.

 

 

Hello Klaus,
that's something I did already previously. I wanted to know if rotation basically should work, and I know the old AxisInterface visualizations, so I got the library and I saw that the frame for the handling of the axis is still used. But my own visualization doesn't work, I don't see any problem in the properties of visualization elements. Nevertheless there is no movement.

 

Goldfinger
Established Member

So i am at the end of my knowledge 😮.

Maybe someone else can help??

Any news here from JoachimS?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist