Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Missing path of recipe manager read/write with PLC V2.04

Missing path of recipe manager read/write with PLC V2.04

alink
New Contributor

Hello,

after updating ctrlX PLC to V 2.04 the recipe manager doesn't save recipes anymore.

No path is created. When creating it manually, it still doesn't work.

Path defined in recipe manager is: PLCLogic\AllRecipes\Programme

alink_0-1706628777425.png

Taking a look on CtrlX with WinSCP via WebDAV it's looking this:

Originally, folders "AllRecipes" and "Programme" didn't exist. They were created manually (normally recipe manager should do this...)

alink_2-1706628919424.png

Going to "Programme" shows that folder is empty and not used.

alink_3-1706629020996.png

Taking a look to ctrlX PLC: Because different folders are used for different recipes, the "StoragePath" is set before saving / reading each time.

But this "Recipe_Manager.SetStoragePath(......)" never gets TRUE !

The code is unchanged from previous ctrlX PLC V1.20 -- currently just the existing code is taken over from 1.20 to 2.04. alink_4-1706629403113.png

What's wrong ?

As I can remember or as I think, the folder tree was looking different with v1.20, wasn't it?

Where to store recipes?

 

 

 

 

1 REPLY 1

alink
New Contributor

Issue located:

After changing from PLC v1.2 to v2.04, the activated "recipe management" was deactivated suddenly.

I think this happened when converting from v1.20 to v2.04 because project is the same as used with v1.20.

No recipe manager is working.

alink_0-1706870877630.png

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist