cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Leave AH mode error - 090F2002/0C570100

Leave AH mode error - 090F2002/0C570100

Xiaoyin
Member

I used the Axisinterface modular for test. The core is  'X3 and drive is ctrlx drive (xcs)'.

The axie can  execute the position moving or velocity moving normally. But everytime when leave the 'ModeAH' command, the error appeared, meanwhile the servo stayed in AF state. The error can be reset. But why this error appeared? How to solve the problem?

Pls refer the pics for details. error.pngcommand.pngplc_version.png

apps version.png

8 REPLIES 8

CodeShepherd
Community Moderator
Community Moderator

As there are several improvements made for such errors in the latest version please use the current release version of the ctrlX PLC Engineering 2.6.5 (including CXA_MotionInterface and CXA_MotionInterfaceUser version 2.6.1.10) as well as ctrlX MOTION app 2.6.6 and check again.

Thank you for reply.

The newest version of 'motion app' is 2.6.5. How could I get the 2.6.6 version?

2_6_3 APPS.png

CodeShepherd
Community Moderator
Community Moderator

It can be found in the official ctrlX Store page

EDIT:

Only the text in the app package in the early adopter area was incorrect. Now the correct version 2.6.6 of ctrlX MOTION is mentioned.

_Beppo
Established Member

Hi,

I'm using Motion App 2.6.6 & PLC Engineering 2.6.2.

And I'm having the same issue, but for me the error is not resettable (even from plc, DL or webserver).

Also, I'm not able to command the axis's mode (it's stuck in AH).

I've already tried to avoid changing the OpMode if the axis is stopping or stopped (AxisStatu.Data.PlcOpenState.stopping), it solved a lot of cases, but this error sporadically pops out and I'm not able to control the axis.

Regards,

GB

CodeShepherd
Community Moderator
Community Moderator

@_Beppo like mentioned in my post above, please use latest ctrlX PLC version including latest CXA_MotionInterface libraries.

_Beppo
Established Member

Halo @CodeShepherd,

I downloaded the lateste PLC version (says 02.06.05 from collab room), but the IDE says 02.06.02.

 

CodeShepherd
Community Moderator
Community Moderator

@_Beppo could you share some of your program code or commanding order, so we can see what you are doing? Which CXA_MotionInterface librariy version is used? Are any opther CXA_Motion or CXA_PLCOpen functions used?

Beware that an AH mode needs explicitly to be switched off, as the drive will also switch to AH and needs to be returned to AF. You could use the mode stopping instead of AH to not have such behaviour.

_Beppo
Established Member

@CodeShepherd  ofc, I've attached the lib's versions below.

Nothing complicated, I just need to call different modes (not sequencially: always passing by an "idle" state). Like: AB -> AH -> "MoveAbs" -> AH -> "Flex" -> AH -> "Flex" -> AH -> "Flex" -> AH....

While developing with v02.06.04 a rexroth tech told me to avoid MoveStop since we were having some issues about it.

Anyway, it's rude, but I think I soved using the fix I've attached below, interlocking every motion mode with "MC_CoolDown_Motion" and the reset command with "MC_CoolDown_State".

Regards,

GB

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist