FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
03-11-2024 02:29 PM
Dear gents,
I have the following problem when using an existing Codesys project and making it run on the X3 hardware. I get the following error when committing:
Please can you give me some hints to fix it.
Solved! Go to Solution.
03-11-2024 02:30 PM
Addtional inforamtion. On the X3 device the follwing licenses are available:
03-12-2024 09:47 AM
So I assume you are using the version 2.4 of the ctrlX OS system and corresponding application apps?
It sounds like a known issue please refer to our official online documentation:
Bug 757800: ctrlX PLC Engineering: Error message "The download was aborted as the control does not h...
03-12-2024 01:54 PM
Unfortunately the described procedure below does not work.
Please find a quick solution.
03-12-2024 02:44 PM
So please give us some information about your system then. Otherwise it is only guessing. You could first of all add a system report (see how to).
03-12-2024 03:24 PM
03-12-2024 03:50 PM
Your app version are quite a mix from version 1.20 and 2.4 what can lead to unintended behaviour and should not be used like that for productive purposes.
Could you also add a screenshot of the PLC logger?
In a last instance you could send me your contact data via a private message so we can follow the steps together, as this is the way to go.
03-14-2024 09:26 AM
Any news on that topic? I've wrote you a PN some days ago.