cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

About byte swap and convert into 16 bits

About byte swap and convert into 16 bits

Chirag03
Established Member

Hello,

 I have %QB0 8 high bits and %QB1 8 low bits .  How can i swap bits %QB0 and %QB1 for  requirment positions in a 16-bit value ? after that i need %QB0 and %QB1 in to 16bits . For that, i need help.

Please see attached pictures for your reference.

Thanks in advance.

4 REPLIES 4

TheCodeCaptain
Community Moderator
Community Moderator

Hi Chirag03,

you could for example swap and combine it by assigning it to an array and accessing it with a pointer, like in the screenshot.

Or using the functions from our library CXA_Utilities, see second screenshot.

TheCodeCaptain_0-1701699586937.png

 

TheCodeCaptain_1-1701699815870.png

 

Thank you very much for your reply.

I did as per your first screenshot . I have to write values in Output byte . because there is a cross connection .  I have error .

Please see attached picture.

 

Hi,

either use the AT operator, or map it in the dialogue, you cannot do both.

Hi ,

Thank you for your reply.

Yes that is true . I only map it in dialogue  . But there is still same error. i can not set into the output bytes .  i have to set into form of 16  bit . 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist