FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
04-22-2022 04:34 PM
Hey,
I was wondering if there is a way to work around the Position limit set inside de MOTION? the current limit is 360000 degrees but this is not enough for my application (see attachment) . In DRIVE i have set the maximum to 107 374.1822 degrees (the maximum amount)
Is there a work around to get rid of all the position limits? or atleast the one set inside the MOTION app in the ctrlX CORE?
Good weekend!
Solved! Go to Solution.
04-26-2022 01:23 PM
At the moment it is not possible to extend this value nor switching the limit off.
You could use a modulo axis. This can also be commanded to greater values then the modulo value e.g. modulo=360deg, command=1000deg, result= 2 turns and 270deg.
I will talk to some colleagues and developers and try to get further information.