cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

node-red: how to send commands, like booting motion, or move axis?

node-red: how to send commands, like booting motion, or move axis?

Kostya
Member

I was trying to send

msg.payload='{"type":"string","value":"Booting"}';

to a "data layer request" node with "WRITE" method, to "motion/cmd/opstate", like in REST method, but to no avail - gives me error "CtrlxProblemError: DL_TYPE_MISMATCH". Does structure of request and destination differs from REST method (and how)?

 

4 REPLIES 4

CodeShepherd
Community Moderator
Community Moderator

This is about sending complex data objects to the ctrlX Data Layer. Please refer to this topic where the mechanism is explained.

Ok. I think, I made code right like in a post. But something wrong still, error persists.

function codefunction codedata layer node parametersdata layer node parameters

CodeShepherd
Community Moderator
Community Moderator

You mentioned two things.

First is switching to booting/running. You have to send a CREATE to the node "motion/cmd/opstate" not a WRITE with this payload:

EDIT:

 

var newMsg = {};
newMsg.payload = {
     "type":"string",
     "value":"Configuration"
     };
return newMsg;

 

 Second sending a movement command via CREATE to "motion/axs/AxisX/cmd/pos-abs":

 

var newMsg = {};
newMsg.payload = {
      "type":"object",
      "value":{
	    "axsPos":"10","buffered":false,"lim":{"vel":"10","acc":"10","dec":"10","jrkAcc":"0","jrkDec":"0"}
	    }
     }
return newMsg;

 

Indeed, using CREATE method solved the problem!

Thank you, very much!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist