FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
05-31-2021 11:37 AM
Hi.
My contrlX Motion app shows the error in subject topic.
Even when there is no axes added.
What can be cause?
Thanks!
Solved! Go to Solution.
05-31-2021 05:53 PM
05-31-2021 06:02 PM
06-02-2021 09:13 AM
To clearify what I mean:
It seems to me that your configuration still contains a connection to an axis.
Motion => Axis Profiles => Make sure there are no profiles
Motion => Axis Configuration => Make sure there are no axis
Do the same for the Kinematics configuration and profiles.
After that save the configuration (Configurations => Save button).
In the configuration file you can check if there are axis in the axisProfile and motion folder.
Otherwise download the configuration to your PC and post it here.
With kind regards,
Leon Paridaans, VHE Industrial Automation
06-02-2021 04:14 PM
06-02-2021 04:27 PM
Indeed no axis nor profiles in the configuration.
Only thing I can think of is just to disable/delete the motion app, as you don't use it anyway?
Maybe the experts can help you out.
06-09-2021 09:17 AM
Could you please tell us which error is shown? Or simply do an system report and add it to this topic?
06-14-2021 03:36 PM
Hi CodeShepherd.
It seemed the ctrlX cycle time was changed, even though I am not aware there was a setting of the cycyle time and how was it changed ?
The problem seems to be resolved after correcting the cycle time. :]
06-15-2021 09:08 AM - edited 06-15-2021 09:17 AM
I am not sure how this corresponds but for your information the cycle time settings of the ctrlX CORE and the PLC: