cancel
Showing results for 
Search instead for 
Did you mean: 

Motion app hangs in Configuration/Running after booting

alink
Established Member

Motion app hangs in Configuration/Running after booting

Hello,

without any change in motion app / axes profile since some days motion app is hanging in Configuration/Running. The only way is to set it to running manually. Then everything is working fine till next time of booting (restart, shut off/on).

The only thing which was changed at the ctrlX was adding a SD-card and doing some PLC code changes. But these don't have this effect.

Diagnostic:

diag.JPG

Axes

motion.JPG

I tried to activate trace but it is not possible to set variables to true....wether in setup nor in service mode.

trace.JPG

Installed apps:

apps.JPG

4 REPLIES 4
CodeShepherd
Community Moderator

Re: Motion app hangs in Configuration/Running after booting

Please, like you also mentioned, try to switch on traces, then save your app data (active configuration), set logbook to persistent and reboot control. Afterwards do a system report so we have all information necessary.

Writing Data Layer values are not limited to an operation mode and should be possible at any time.

alink
Established Member

Re: Motion app hangs in Configuration/Running after booting

Trying activating trace but it's not possible. Can't write the parameters.... wether in service, configuration or run mode..

datalayer.JPG

CodeShepherd
Community Moderator

Re: Motion app hangs in Configuration/Running after booting

I already saw you picture above. But it just shows that you have entered (or it was already entered) "false". "Write" and "Discard" buttons stay gray/disabled as long the value in the window above do not change. So just overwrite "false" with "true" and then they will get active.

alink
Established Member

Re: Motion app hangs in Configuration/Running after booting

Ah, sorry, didn't know that it is possible to write / type directly into that field. Yes, after renaming 'false' to 'true' it's poosible to 'write'.

So, now there is a app-data-archive and a diagnostic log. Hopefully that contains the needed information to solve that issue.

As said, after switching to running everything is working fine without any issue whole day long.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist