Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

IDE app - error 1234 when motion is initialized

IDE app - error 1234 when motion is initialized

Yvonne_
Established Member

Hello,

I run into a problem with the IDE app (V1.14.3): As soon as I configure/initialize the motion (axis and/or kinematic) in a project, it will not run anymore and the error '1234' appears, also if there aren't any motion commands in the code.

When I remove the configured axes, the program runs normal. Initialization of the axes is possible without problems, and the axes can be moved in the commisioning mode of the ctrlX webinterface. Reïnstalling the IDE/python app does not help. 

What could be going wrong here?

YvonneV_0-1655907908580.png

 

File "/var/snap/rexroth-automationcore/common/solutions/activeConfiguration/scripts/bosch/tiger/d070fbe9-a9ae-4b20-29d5-e2bcc96bfa2c.py", line 911, in [main]
File "/var/snap/rexroth-automationcore/common/solutions/activeConfiguration/scripts/bosch/tiger/d070fbe9-a9ae-4b20-29d5-e2bcc96bfa2c.py", line 912, in motion
File "/var/snap/rexroth-automationcore/common/solutions/activeConfiguration/scripts/bosch/tiger/d070fbe9-a9ae-4b20-29d5-e2bcc96bfa2c.py", line 737, in create_axis

3 REPLIES 3

CodeShepherd
Community Moderator
Community Moderator

Did you have a look to thee ctrlX CORE logbook?
Which error is generated there?
Are you using low motion functions and the state of the motion does not fit to the command?

Your program will be compiled to a single script file. You could also have a look in this script in the app data what happens in the lines that are mentioned by the error.

Are there any news or can this topic be closed?

Hi, I could not find a clear cause of the error in the script file/log book/... - in the end I did a new installation of the core (back to factory settings and re-install all apps), this seems to have solved the issue. Thanks for your support!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist