FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
09-12-2022 10:55 AM
Hello,
A customer is making an application with two Axes, DriveX, Motion app, AxisInterface and Webvisu.
he is having problems with task configuration and AxisInterface initialisation.
Currently you have it configured as picture "error 1", with the 10ms FastTask task calling the AxiInterface cyclic.
The problem is that sometimes when starting the PLC or loading the program the AxisInterface does not initialise and has to do a warm reset several times (error2).
It also happens that when partially downloading the program the AxisInterface of the Axes indicates an error without the Drives are in error or the PLC, it happens during the download program (Error3).
Could it be a problem of task times, priorities or programme calls that do not initialize well?
Thanks in advance
Solved! Go to Solution.
09-12-2022 05:11 PM
It looks like the axes are configured correctly in the axis interface. Could you provide the error information of the TE_AxisInterfaceMainProg (ErrorID: ERROR_CODE, ErrorIdent: ERROR_STRUCT)? There is mentioned what is going wrong.
09-15-2022 05:31 PM
Hello CodeShepherd,
Attached image requested when the AxisInterface has not initialized.
It is strange because it does not show any error.
Anyway, the client tells me that to force the AxisInterface not to initialize, what it does is to lower the time of the task call to 4 ms. If you set it to 10ms it works correctly.
What is the recommended time for the AxisInterface task? Is it recommended to go below 10ms?
Thanks.
09-16-2022 07:23 AM
We will check this. Could you also tell the version of the ctrlX MOTION app and the CXA_Motioninterface you are using?
09-16-2022 08:47 AM
The customer is using the latest system image V1.16 and as PLC software has installed the version currently available for download in the Collaboration Room 1.16.
The software was installed 2 weeks ago.
09-19-2022 03:41 PM
We could not reproduce the errors as that you got. Would it possible to send me a private message with your contact data so we probably could do a meeting or share the project?
09-20-2022 12:02 PM - edited 09-20-2022 12:02 PM
Hello CodeSheperd,
I have sent you the project so that you can replicate the error.
Thanks
09-27-2022 02:22 PM
Project is running now. Please contact us again if you need further help.