FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
05-27-2021 04:31 PM
after pressing the emergency stop the drives go into STO. after STO is lifted what is the correct way to return the axes to ModeAH/AB?
The axes now remain in "DISABLED" after STO. with a relatively simple command such as: arAxisCtrl_GB[AXIS].Admin._OpMode := ModeAH it does not work.
I am looking for a way to do this through my PLC APP.
Solved! Go to Solution.
05-31-2021 08:47 AM - edited 05-31-2021 08:51 AM
Does this happen with every STO situation ?
The correct situation : If the ctlX drive is not enabled, you should be able to go to STO and back without any problem.
The faulty situation : If the drive was enabled and then go to STO would/should trigger an error. This error muts be released before the PLC motion can go back into AH. Inside the motion function block could be an error triggered which have to be resetted first. ( This can, for example happen after a E-stop when the delay time f is too short, and the STO switch is with the drive still in AH)
06-14-2021 02:28 PM
Any news from your side AndroidzZ?
06-15-2021 07:51 AM
the problem arose from a faulty relay. After replacing the relais everything worked as intended.