Telegraf 1.18.9 Error

Telegraf 1.18.9 Error

bkautzman
Established Member

It seems that between Telegraf 1.18.7 and 1.18.9 a bug was introduced relating to multiple subscriptions. After updating to 1.18.9, I receive the following error when starting the configuration:

Creating sse client to subscription 2: failed to create sse subscription 2 status: 401 Unauthorized;web.telegraf;

I have 4 subscriptions configured. It's not always subscription 2 that causes the issue, it can be any of the other ones individually or even multiple at once. Occasionally there is no issue, but this happens infrequently.

I've attached my configuration for 1.18.7 and 1.18.9, as well as the diagnostic log showing several of the errors.

 

 

6 REPLIES 6

MauroRiboniMX
Contributor

Hello Can you provide our configuration? 😊

Hello Mauro,

Which configuration are you referring to? I've attached the config files for Telegraf to my initial post.

Your automation core and other apps version 🙂. It is really important to align all the apps 🙂

I was able to reproduce it. 😃

I opened a bug to see if that is a bug or just not the right approach. I would make anyway 2-3 different configurations and not multiple subscriptions in one configuration. 

Should be fixed with the next release 🙂 

Thank you Mauro!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist